6/23/2011 11:02 PM | |
Posts: 344 Rating:
|
Rataplan, It is not a fixed de-rating number. Motor rating will depend on the speed range that you will be operating the motor at. It is represented by the torque/speed curve of the motor. I included an example curve of the 1LE1002 motor. The easiest way to pick the right size motor and drive is to use Sizer program. It will consider the operating range that you specify and recommend appropriate motor and drive. The torque curve, that I included, is output right from the Sizer program. It considers other factors as well: incoming voltage, drive efficiency, installation altitude, etc. |
Last edited by: DenisMor at: 6/23/2011 11:02 PM |
|
Follow us on