10/3/2010 6:34 PM | |
Posts: 95 Rating: (1) |
Hi, Ihave some problem with communication of CU240-PN with 1)Sinamics CU 320 : We are using C240PN for conveyor control. There are 3 nos of CU320 on profibus which is connected to X9 ( DP) port of C240PN. There is BUS fault 2 is coming. But we can see all addresses in Scout. When we open hardware configuration, there is only C240PN is online but not CUs. [schnippschnapp] I hope i ll overcome my problems. Regards, JD Splitted from G120 to AB via Ethernet. |
Last edited by: O_Moderator at: 10/4/2010 11:00 AMnew subject after splitting |
|
10/5/2010 2:48 PM | |
Joined: 7/28/2010 Last visit: 3/18/2024 Posts: 184 Rating: (11) |
JD, Can you see all drives through Scout? Do you go online with hardware config through Ethernet or Profibus? Regards, Behnam CPU315 <-> S120, How????? |
10/8/2010 7:50 PM | |
Posts: 95 Rating: (1) |
Hey we are in a BIG problem can sombody help..????? Its communication with C240PN Regards, JD |
10/8/2010 8:23 PM | |
Joined: 7/28/2010 Last visit: 3/18/2024 Posts: 184 Rating: (11) |
JD, If you need help, you should give more information. Regards, Behnam www.sigmaprocess.ca/blog |
Follow us on