1/14/2022 9:14 AM | |
Joined: 10/10/2005 Last visit: 8/29/2024 Posts: 1917 Rating: (136) |
Hello Shahab_6448015, perhaps the following information will help you. The sequencer switches to the next step as soon as the conditions in the transition are fulfilled again. Or you can use the initial step to return to the beginning of the sequencer. You can also define the initial step in the middle of the step chain. You can also program queries from the instance DB in the structure of the transition. These are the parameters TV, TT and TS. An example can be found in the FAQ: What tips and tricks are there for executing and monitoring steps and transitions in S7-GRAPH V5? With best regards |
Follow us on