10/11/2013 2:18 PM | |
Joined: 3/14/2010 Last visit: 9/4/2024 Posts: 359 Rating: (5) |
Hello, everybody ! I uploaded the program from PLC S7-200 (CPU 224XP) and then ONLY corrected the program in 6 networks at a Program Block (SBR21) and made nothing more. I didn’t change anything in hardware and other configuration at all. Now I want to download the corrected offline program back to PLC. But the following message appears "There are wizard configurations that do not match for attached modules. Reposition Intelligent modules or exit and reconfigure using the wizards". See "Attachment: Ether_01.GIF" above or here /tf/WW/en/postattachments/download?attachmentId=29234 Why do I get the warning ? What does it mean and may I continue downloading ? Will the PLC program work properly after that ? Thanks in advance. |
Last edited by: Alex3110 at: 10/12/2013 7:30 AMLast edited by: Alex3110 at: 10/12/2013 7:15 AMLast edited by: CS Moderator at: 10/11/2013 4:23 PMnew subject after splitting from /tf/WW/en/Posts/75975#top |
|
This contribution was helpful to1 thankful Users |
10/14/2013 8:02 AM | |
Joined: 3/14/2010 Last visit: 9/4/2024 Posts: 359 Rating: (5) |
Hi, Marcjan ! You were right in your first post. But this picture (see /tf/WW/en/postattachments/download?attachmentId=29234) is not from my PLC. I took it from another Topic as an example to show the warning text. Because the following reason : - the PLC program creator was not me ; - I had not a sufficient skill to work and to program the S7-200 completely I didn’t find at once that the program included the Ethernet CP-module Wizard. Who could know that the above mentioned Wizard was located in the Data Block Project Folder ? In fact there is no any СР243-1 module (Ethernet) in my PLC. Bad boy forgot to delete the Ethernet CP-modules Wizard from the Project and I had a trouble this time Thanks. Now everything is clear. |
Last edited by: Alex3110 at: 10/14/2013 8:11 AMLast edited by: Alex3110 at: 10/14/2013 8:08 AMLast edited by: Alex3110 at: 10/14/2013 8:03 AM |
|
This contribution was helpful to1 thankful Users |
2/18/2016 3:43 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating: (122) |
New question published by vsubbu is split to a separate thread with the subject Configure an Ethernet module in S7 200. Best regards |
Follow us on