1/23/2012 1:10 PM | |
Joined: 8/31/2010 Last visit: 7/2/2024 Posts: 1517 Rating:
|
Hello glinglin, You need to synchronize date and time of S7-1200 with the KTP 600 Mono Basic Panel. Check here on- How do you synchronize the time of the HMI Basic Panel with an S7-1200 PLC? This is a STEP 7 v10.5 project and you directly open in STEP 7 v11 SP2. It will convert into the suitable format and then you can make use of it. There are many other threads in this forumspeaking aboutthe Time Synchronization of S7-1200 and SIMATIC HMI Basic Panels. |
Like it? Rate it! |
|
This contribution was helpful to
1 thankful Users |
6/27/2012 9:15 AM | |
Posts: 1 Rating:
|
Thanks for this, also been looking these last couple of days to synchronise the trend view date/time with the PLC. |
Follow us on