2/22/2024 4:18 PM | |
Joined: 9/23/2005 Last visit: 6/14/2024 Posts: 4575 Rating: (706) |
It is described in SINAMICS S120 Function Manual . |
Regards, |
|
2/23/2024 12:54 PM | |
Joined: 8/2/2018 Last visit: 6/5/2024 Posts: 11 Rating: (0) |
I've checked the specifications of the cogging torque compensation function but I'm not sure it suits my needs. The manual says that this is to reduce the cogging torque at low speed but if I rotate the motor at low speed (1 rpm) there is no cogging or ripples in its velocity. I experience cogging only when the motor operate in torque limit. I suppose this is due to the fact that its p1300 is = 22 (speed control with encoder), probably by using close loop torque control I obtain a better beahviour. What do you think about it? |
Follow us on