8/24/2025 11:28 AM | |
Joined: 12/18/2014 Last visit: 9/16/2025 Posts: 35964 Rating:
|
S7-PCT V3.5 SP4 for IO-Link MasterThe Port Configuration Tool ("PCT") is a PC-based software for parameterizing Siemens IO-Link Master modules and third-party IO-Link devices. The IO-Link devices are integrated using the "IODD" standardized device description which can be obtained from the relevant device manufacturer. S7-PCT supports both IODD versions 1.0 and V1.1. |
This contribution was helpful to
1 thankful Users |
Follow us on