12/1/2022 10:52 AM | |
Joined: 5/6/2022 Last visit: 7/16/2024 Posts: 431 Rating:
|
Hi JLindsay, To see what might be happening and why this failure has occurred we would appreciate it if you could share the following information with us: - First of all I recommend that you go through the following FAQ step by step as it is vital to have it set up correctly: "What are the requirements for the use of SIMATIC WinCC in a Windows network?" - Screenshot of the operating system (OS) you are working on the client by accessing from the Windows bar command "Winver". - Screenshot of the error you get. - Have you made or have there been any changes recently? Any software updates, windows updates or IT changes? Best regards! |
If this Information really helps, you could use the Rate function |
|
3/20/2024 9:39 PM | |
Joined: 5/12/2023 Last visit: 7/1/2024 Posts: 1 Rating:
|
Me too! The same problem. Would be great if Someone of us shares right solution if figure out. |
Follow us on