7/30/2021 12:16 AM | |
Joined: 11/26/2016 Last visit: 10/8/2023 Posts: 138 Rating:
|
Hello every One; I have a machine Operated with simunerik 840c CNC system connected with 611A Drive System. The Drive Configuration is attached. The question is Can I replace spindle drive shown with siemens sinamcs one (stand alone one with its own 600vdc supply) with an analog reference input voltage? Is the drive system operated well if I remove the spindle drive from the drive chain? Does the drive system make check on it self so that it will start the axis drives if I remove the spindle drive? The control signals of the spindle is also attached. Thanks.
AttachmentDrive Configuration.pdf (917 Downloads) |
Nothing IS IMPOSSIBLE. |
|
7/30/2021 5:43 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, 1. Yes you can replace your 611A analog drive with Sinamics. 2. Can it operate on 600V DC bus of present 611A drive bus - Answer is NO. 3. Can I remove spindle drive & run system - NO. To replace 611A drive with Sinamics you need CU310-2DP 6SL3040-1LA00-0AA0, Sinamics converter 6SL3210-1SE31-1AA0, SMC10 module 6SL3055-0AA00-5AA3. Please note, with CU310-2DP you need to connect on Profibus with NCU & it can control single axis only. Sinamics converter needs 3 phase AC 380-480 V AC supply (here I presume it as your AC input supply range. If it is other than it, you need to select appropriate converter module) SMC10 is to connect your motor encoder to drive. CU310 has onboard Analog & digital inpputs which you can configure. Please note, since 840C is old NCU, you need to confirm connectivity & communication compatibility of 310CU witg NCU on Profibus. For this you may contact your nearest Siemens support center. HTH. |
7/30/2021 9:09 AM | |
Joined: 11/26/2016 Last visit: 10/8/2023 Posts: 138 Rating:
|
|
Nothing IS IMPOSSIBLE. |
|
8/7/2021 10:11 AM | |
Joined: 7/18/2020 Last visit: 12/17/2023 Posts: 46 Rating:
|
Hello Nulizhang, User A.Elmawgoud wanted to know if it is possible to replace 611A drive by Sinamics drive just by connecting it to present drive system, retaining spindle motor as it is. PISCEAN2010 reply is - yes it is possible but Sinamics drive cannot be connected to present drive system. It needs new CU with Sinamics S110 AC-AC drive retaining spindle motor as it is. But it needs modification in present PLC as well as NC MD data. (Spindle motor with encoder) will be retained as it is. PISCEAN2010 - please correct me, if I am wrong. HTH |
This contribution was helpful to
1 thankful Users |
Follow us on