6/30/2009 8:24 PM | |
Posts: 204 Rating:
|
OSCAT stands for "Open Source Community for Automation Technology". OSCAT is a Open Source library according the IEC61131-3 standard. The OSCAT.lib is present in Open Source and is as a Framework for applications in automation. the OSCAT.lib contains more then 800 modules from the ranges * Mathematics * String / List / Buffer * Logic * Time/Date * control * signal processing * HVAC * Building Automation * Networking * Automation / Control * Device Drivers The library as well as the documentation are available in the download area under www.oscat.de. |
This contribution was helpful to
8 thankful Users |
6/30/2009 8:25 PM | |
Joined: 12/20/2008 Last visit: 9/3/2025 Posts: 556 Rating:
|
Thanks for information |
Follow us on