9/25/2020 11:16 AM | |
Joined: 11/27/2018 Last visit: 4/12/2023 Posts: 7 Rating:
|
Hello, I am currently working on a redundancy setup almost similar to what ahbishek has described ( two CP-8050 master modules, each with a CI-8520, a base I/O and a remote I/O where the two master modules are to be synchronized via an IP based synchronization interface on CI-8520). I have gone through the manual for the redundancy configuration for the CP-8050 but I am struggling with the following in the configuration process; 1. Defining redundant processing firmware. 2. Testing the synchronization function to test the whole redundancy function. Ahbishek, may you kindly assist me if you have managed to implement your redundancy successfully or if there is anyone else who can assist me in implementing this setup. Kind regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/28/2020 10:32:14New subject after splitting |
|
This contribution was helpful to
1 thankful Users |
Follow us on