1/7/2025 2:32 PM | |
Joined: 11/18/2024 Last visit: 1/24/2025 Posts: 10 Rating:
|
I did another research and there was a similar problem before. Here is the link to the forum thread and in last post there is an answer. Support packages can be found here. It now allowed me to upload whole PLC hardware, and theoretically also software without any errors, but still it shows me that my version is 4.3 and online 4.5. Also all circles next to the program blocks are half blue and half orange meaning there are some differences between them, even though the upload was complete (language en_US (offline) and es_ES (online). May I change it to 4.5 somehow? May I change any block and download it without breaking the PLC program (I have now online view in RT)? |
Last edited by: AutoGen_2769615 at: 01/07/2025 14:34:03Last edited by: AutoGen_2769615 at: 01/07/2025 14:34:44Last edited by: adanes at: 01/07/2025 14:57:36 |
|
1/7/2025 3:35 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, Please have a look at the following links: Release S7-1200 CPU Firmware version V4.5 See compatibility: ************************************************************** An S7-1200 CPU with version 4.5 is replacement compatible with an S7-1200 and firmware version 4.0, 4.1, 4.2, 4.3 and 4.4. This enables the use of a real existing CPU with firmware version 4.5 with an engineered V4.0, V4.1, V4.2, V4.3 or V4.4 based on an existing TIA portal older versions project. The new firmware features cannot be used in that case. ************************************************************** And Conclusion: The firmware of CPU is v4.5 Using TIA Portal v15.1 the project uses FW v4.3 (Latest one for v15.1) (You can not change the firmware version to v4.5 using TIA Portal v15.1 The colored circles (Blue/Orange) can be because of Date/Time stamp Best regards, Wizard |
This contribution was helpful to
1 thankful Users |
Follow us on