8/28/2017 7:36 PM | |
Posts: 6 Rating:
|
hi everybody! i have cpu 1214 dc dc dc v4.0 and have a servo motor, i don't know how to connect from driver servo to PLC to use HSC. you know, driver servo have 4 pin, they are: CHA+, CHA-, CHB+, CHB-. i use HSC1 in my PLC, so I0.0 is CHA phase, and I0.1 is CHB phase. Then i connect CHA+ with I0.0, CHB+ with I0.1, CHA- and CHB- with 0VDC from 24VDC power. But i can't read any hsc value. so i think i don't know how to connect plc and driver to use HSC. do you help me? it will be helpful for me. thank you so much! ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 9/8/2017 8:32:51 AMDeleted personal information Last edited by: The Helping Hand at: 9/8/2017 10:15:42 AMNew subject after splitting |
|
9/8/2017 10:50 AM | |
Joined: 8/21/2014 Last visit: 9/12/2025 Posts: 1087 Rating:
|
Closed, cause question posted twice. The second thread with the subject hsc help is published within the conference SIMATIC S7-1200. Best regards |
Last edited by: Jen_Moderator at: 9/20/2017 11:26:26 AMInserted right conference. My Forum is the place to personalize your profile, |
|
Follow us on