10/10/2024 1:24 PM | |
Joined: 10/10/2024 Last visit: 5/15/2025 Posts: 3 Rating:
|
I WANT TO RUN MPG ON S7-1200 PLC DC/DC/DC. I NEED TO CONTROL TWO SERVO USING MPG |
10/11/2024 10:24 AM | |
Joined: 8/13/2015 Last visit: 12/4/2024 Posts: 87 Rating:
|
Regarding MPG - you can connect it as regular encoder to two Hi speed inputs configured as up-down counter. Configured as quadrature (AB-phase) inputs. Some info there. BTW MPG can be with Hi level outputs (up to 24V), low voltage 0-5V or differential RS485 level. Depending on this you need to select corresponding input module/PLC. All other things/connections depends on used hardware which is not mentioned. |
Last edited by: Romasxp at: 10/11/2024 10:27:17 |
|
This contribution was helpful to
1 thankful Users |
Follow us on