11/3/2023 4:02 AM | |
Joined: 3/30/2020 Last visit: 9/5/2024 Posts: 4721 Rating:
|
Hello. Have a look at the manual provided here: [LINK: SIMATIC STEP 7 S7-1200 Motion Control V6.0 to V7.0 in TIA Portal V16]. The status of the motion can be read directly from the DB that is created for the motion control. There are instructions available to read / write some of the parameters such as acceleration / deceleration. Do note the measurement units used. Already helpful? ~ |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
1 thankful Users |
11/8/2023 11:21 AM | |
Joined: 10/25/2023 Last visit: 12/9/2023 Posts: 6 Rating:
|
It helped a lot, thank you! |
This contribution was helpful to
1 thankful Users |
Follow us on