12/11/2012 9:22 AM | |
Posts: 14 Rating: (1) |
Dear All, For one of the project requirement iswith respect to F-System (F-CPU ) is complaint with requirements. The same have been enclosed herewith. The system will be installed in Middle East. Kindly, let us know the S7 400 FH complaint with this requirements. Thanks and Regards, Amol Das AttachmentS7 400 FH Codes and Standards Certification.pdf (1078 Downloads) |
12/12/2012 4:07 PM | |
Joined: 9/27/2006 Last visit: 10/13/2024 Posts: 12287 Rating: (2685)
|
Hello Amol Das; Information on approvals and standards used in Siemens automation equipment are found in a variety of documents. For example, the attached file shows certificates applicable to all Siemens S7-400 CPUs, and are therefore applicable to S7-400H/FH models. It covers CE (Low voltage, EMC and Explosion Protection directives), UL, CSA. FM (Class 1, Div 2, Groups A,B,C.D),EM 61000-x, and Ex approvals. It is taken from the following manual: SIMATIC S7-400 S7-400 Automation System Module Data You will also find compliance to NAMUR standards for the power supplies of the S7-400 in the same manual. For data on the SM 326-1RF00=0AB0 Safety 8 DI x NAMUR module: SIMATIC Automation System S7-300 ET 200M Distributed I/O Device Fail-safe signal modules For a list of functional safety certificates in S7 Safety PLCsc( covers IEC 61508 and more): Functional Safety/Safety of Machinery, Type Examination Certificate, TÜV (see note 3) Release of Failsafe Operation for Innovated S7-400H CPUs Safety Engineering in SIMATIC S7 This FAQbriefly mentions NFPA 72 compliance for a F-DO module 6ES7326-2BF10-0AB0: Using the "Hold last valid value" function of F-DO 6ES7326-2BF10-0AB0 can you achieve an SIL in compliance with IEC 61511, IEC 62061 or a PL in compliance with ISO 13849-1? SIMATIC Industrial Software Safety Engineering in SIMATIC S7 (see the following extract) AttachmentC:\Users\chard2\Documents\SForm\S7-400 standards, certificates and approvals.pdf (814 Downloads) |
Last edited by: dchartier at: 12/12/2012 9:13 PMLast edited by: dchartier at: 12/12/2012 5:31 PMLast edited by: dchartier at: 12/12/2012 4:09 PM |
|
This contribution was helpful to3 thankful Users |
Follow us on