12/5/2017 8:50 AM | |
Joined: 3/20/2017 Last visit: 11/16/2023 Posts: 140 Rating:
|
Is it possible to turn off the FORCE led in the S7-300 PLC even when I have active forces? |
7/20/2023 6:13 PM | |
Joined: 1/22/2023 Last visit: 4/20/2024 Posts: 2 Rating:
|
Force LED is blinking! What does that mean? |
Last edited by: Alef Y at: 07/20/2023 18:34:16 |
|
7/23/2023 6:37 AM | |
Joined: 5/28/2008 Last visit: 9/7/2024 Posts: 4515 Rating:
|
Hi, It means that you are in "Node Flash Test Mode" In this mode FRCE led flashing with 2 Hz frequency See point # 6 in the following link. Tips and tricks for loading and testing S7 programs And see page 22 in the attached pdf to this link SIMATIC S7-300 CPU 31xC and CPU 31x: Technical specifications Hope this helps. |
Ayman Elotaify |
|
This contribution was helpful to
1 thankful Users |
Follow us on