Industry Online Support
Technical Forum
12/15/2022 11:34 AM | |
Joined: 3/11/2019 Last visit: 9/4/2024 Posts: 1564 Rating: (286) |
Hi maksim_d163, you have to change the hardware configuration. But if hw config is changed, you can use the io modules on both interfaces. What are the differences between the Basic (BA), Standard (ST), High Feature (HF) and High Speed (HS) modules of the ET 200SP and ET 200MP?" All ET 200SP IO modules can be used on all ET 200SP interface modules.Exception:
regards sancruz |
Last edited by: sancruz at: 12/15/2022 11:38:30Feedback appreciated, please rate |
|
This contribution was helpful to1 thankful Users |
Follow us on