8/12/2024 3:45 PM | |
Joined: 1/16/2021 Last visit: 8/12/2024 Posts: 5 Rating: (0) |
Hello I am new to step7 How do you import a cfg file in step 7 or Tia-portal? ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 08/13/2024 07:41:05New subject after splitting |
|
8/13/2024 8:37 AM | |
Joined: 5/29/2024 Last visit: 9/17/2024 Posts: 63 Rating: (10) |
Hi Alejandro Panto! In TIA PORTAL, to export hardware configurations, gsd or gsdml files are used. In the following link you can find information on how to install them. The way to import a cfg in STEP 7 is from an already created station, select Station > Import and select the cfg file. The cfg files are no longer used in TIA PORTAL. In TIA Portal it is not possible to import a hardware configuration from Step7 V5.x. For information on how to implement a migration and which prerequisites must be observed, see the following link: Which requirements must be met to migrate a STEP 7 V5.x project to STEP 7 Professional (TIA Portal)? |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to2 thankful Users |
Follow us on