3/28/2017 11:41 AM | |
Joined: 3/28/2017 Last visit: 9/12/2025 Posts: 2 Rating:
|
We have one of the above motors which we bought from DMG as new. After a year of using this motor we started getting errors. To make sure the problem was from Motor we exchanged the motors between two machines and our problem was transfered. SO we are sure out motor has something wrong in it. We think the problem is from the encoder. Motor will run sometimes without any problem. The problem shows when we are running the driven tool in our CNC machine at 4000 rpm and than lowering it the motor will stop after a while. We think the problem is caused from the encoder. I have added an extra earth wire and this reduced the problem. Can we receive an address in order to send the motor to siemens for repair or to be checked . ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/28/2017 4:32:05 PMNew subject after splitting |
|
Follow us on