Industry Online Support
Technical Forum
2/3/2020 4:31 AM | |
Posts: 3 Rating:
|
Dear Expert! I am currently using the Multiturn absolute encoder FVM58, gray code. I would like to modulate the signal of the encoder from 0-8192 to 0-360 degrees. However, I had the difficulty that is after connecting and programming, the encoder rotated to increase from 0 to 8192, then decreased from 8192 to 0. The Correct rotation must be 0-8192 then repeat the same cycle. With the Multiturn absolute encoder FVM58, binary code, I'm writing structure as "and", with the Multiturn absolute encoder FVM58, gray code, I am using the structure "xor".
Attachmentencoder.pdf (238 Downloads) |
Last edited by: DungDC at: 02/03/2020 04:46:52 |
|
Follow us on