6/15/2011 11:31 AM | |
Joined: 4/24/2006 Last visit: 10/10/2024 Posts: 8745 Rating: (1168) |
Hello, Try to search. See this link: http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=6ES74000HR004AB0&caller=view Best regards, Wizard |
This contribution was helpful to1 thankful Users |
6/15/2011 11:51 AM | |
Joined: 7/2/2008 Last visit: 9/30/2024 Posts: 928 Rating: (308)
|
Hello Automation Way, As far as I know there's not certain document/link that gives you individual MLFBs for any bundle selected under S7-400 (I think it's also the same in PCS7 bundles). As stated by Wizardyou will have toexert some effort every time you want to know MLFBs in a certain bundle. I can give you them quickly but you will have to change some MLFBs when you change your bundle (e.g. CPU 414 instead of 412, 4MB Ram instead of 1MB and so on). For your 6ES7 400 0HR004AB0, (SIMATIC S7-400H, 412-3H SYSTEM-BUNDLE H-SYSTEM ) WITH 2 X MC 1MB RAM, (6ES7952-1AK00-0AA0)
1 X UR2-H, (6ES7400-2JA00-0AA0) 2 X PS407 UC120/230V, 10A (6ES7407-0KA02-0AA0) 4 X SYNC-MODULE 10M (6ES7960-1AA04-0XA0) 2 X SYNC-CABLE 1M (6ES7960-1AA04-5AA0) 2 X CPU 412-3H (6ES7412-3HJ14-0AB0) 4 X BACK-UP BATTERIES (6ES7971-0BA00) Best regards. H-H |
This contribution was helpful to1 thankful Users |
7/7/2011 2:49 PM | |
Joined: 8/18/2009 Last visit: 6/17/2024 Posts: 548 Rating: (33) |
Thank you for your reply |
Rajkiran Patil |
|
7/8/2011 4:49 PM | |
Posts: 2 Rating: (0) |
Export to HW feature is much help. Thank you. |
Follow us on