Industry Online Support
Technical Forum
1/19/2009 12:01 PM | |
Joined: 1/4/2007 Last visit: 6/13/2024 Posts: 1131 Rating:
|
Hello Alin, The RS232 communication is not publicised from Siemens. But if you only want to read the weight values, I recommend you to use the TTY-interface. The TTY-protocol is decsribed into the “old” Siwarex U manual (see also the attached file, chapter 11.1, Table 11-7). The TTY-protocol is a STX/ETX-protocol, and more easier to handle than the RS232-protocol. If you are using the TTY interface, you need a TTY/RS232-converter for the PC. Best regards Siwarexi AttachmentTTY-protocol.pdf (363 Downloads) |
Follow us on