2/15/2012 7:23 AM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating: (86) |
Hi well Mario Braganca is right in one way that the Flexible panel shall have a hardtime switch between CPU if you Use MPI or Profibus. But if you use Ethernet then switching can be automatic. I have used MP277 panel with H system and switching was bumpless. Find the link Please find the attached program for the same. I found this application in siemens FAQ but i do not remmeber the the ID. Have fun... AttachmentMP_277 ON H-CPU.zip (248 Downloads) |
Jazz |
|
2/15/2012 1:07 PM | |
Joined: 1/12/2011 Last visit: 3/13/2024 Posts: 68 Rating: (0) |
Hi Guys, We will use profibus between CPU 400 and ET200M communications only. PC, HMI with CPU 400 are connected by Ethernet TCP/IP. I attached the HW/Network configuration file. Import it to Simatic to check if anything is wrong. Thanks a lot!! AttachmentSIMATIC H Station(1).zip (242 Downloads) |
2/15/2012 7:27 PM | |
Joined: 1/12/2011 Last visit: 3/13/2024 Posts: 68 Rating: (0) |
Dear Tagolover, I checked your program and I have a doubt. I think that ethernet port from CPU 315-2 needs a TCON_PAR block (DB or UDT) to works or not?? |
Follow us on