9/6/2013 9:22 AM | |
Joined: 1/21/2013 Last visit: 10/8/2024 Posts: 4620 Rating: (708) |
Hi jm1983, maybe you can help if it is the fault of the battery: Changing a battery of PLC S7-400. |
9/6/2013 6:06 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715)
|
Hello, First let me tell you i''m not a H-system expert, but it seems strange to me too that if one CPU loses it''s program the other one does the same trick, it may be that the 2nd CPU will not run, but the program must still be in it. Unless someone comes up with a smart answer i would go for a Support Request Meanwhile can you give us a complete discription of the hardware you have there? Regards, Marcjan |
Problem solved? |
|
Follow us on