7/23/2019 7:01 PM | |
Joined: 12/29/2012 Last visit: 9/17/2024 Posts: 120 Rating: (15) |
Hello all, we are having following hardware:- CPU s71500 T, TR Electronic encoder supported standard telegram 81, and sew Movitrac drive. we configure positioning axis Like this, Drive interface Data connection Data Block Telegram used in data block Standard telegram 1 . I Mapped the status bit to Data block standard telegram bits correctly , but still i am not getting the ready signal in control panel. What are the status bits are essential to make power On NoSpeedDeviation ControlRequested SpeedComparisonValusReachedExeeded TorqueLimitNotReached OpenHoldingBrake NoMotorOvertemperature ActualSpeedPositive NoPowerUnitOvertemperature ReadyToSwitchOn ReadyToOperate OperationEnabled FaultPresent NoCoastStopActivated NoQuickStopActivated SwitchingOnInhibited AlarmPresent kindly find our config AttachmentSiemens Forum.docx (595 Downloads) |
Best regards |
|
Follow us on