2/28/2016 3:30 AM | |
Posts: 6 Rating:
|
Hello, The servomotor 1FK7063 is coupled to a table the rotates 180 degrees every 6 minutes, on the rotary table holds a cylinder block and a robot grinds part of the block. The servomotor and the power cables that feed the motor have been overheating, even after it is at rest. When we put a direct air hose to the motor, it cools down and the fault isn't present anymore. We want to do the following tests: Any other suggestions are welcome. I have annex a copy of the program, the servo name is TAV_B.
AttachmentRoboGrind.zip (344 Downloads) |
3/10/2016 6:45 PM | |
Posts: 6 Rating:
|
The air cooling hose was arrange by maintenance workers of the factory.
Regards. |
Follow us on