5/16/2022 8:11 AM | |
Joined: 10/11/2006 Last visit: 9/8/2025 Posts: 6039 Rating:
|
Dear Jom64, First, please find here "Methods of measuring temperature" Here you see, that temperature measurement it self by a PTC is almost not possible, due to its steep curve. A typical PTC evaluating device (e.g. SINAMICS control unit) gives at a dertemined Ohm value (>1610 Ohm) an accordingly signal. Second motor temperature: The base temperature of a el. motor is ruled, it is at 40°C environmental temperature. The motors isolation is split in certain classes in industrial usage mostly B and F and it is stamped on the motors name plate Details are found there: "Thermal classes" When the motor turns comparatively slow the cooling impact of the rotor mounted ventilator is comparatively less, hence it might be possible, that windings temperatur is a little bit higher. But the PTC will trip anyhow at its destinated temperature.
|
With best regards, |
|
5/19/2022 1:20 PM | |
Joined: 7/18/2020 Last visit: 12/17/2023 Posts: 46 Rating:
|
Link is not operational/available. |
Follow us on