12/13/2011 9:06 PM | |
Joined: 9/27/2006 Last visit: 8/5/2024 Posts: 12273 Rating: (2680)
|
Hello Muhammad; Profibus-DP master-slave connections between 2 CPUsare common, easy to configure and require very little programming (only moving data between the DB area and thew input/output addresses of the CPUs). Look at the following sample program showing the simplest form of setup (both CPUs are in the same program): DP link between CPU 315-2DP (slave) and S7-400 (master) with STEP 7 V5.3 Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on