8/14/2024 5:01 AM | |
Joined: 3/11/2019 Last visit: 10/18/2024 Posts: 1622 Rating: (300) |
Hi, the firmware is backwards compatible. So yes. How do you load a project into an S7-1200 CPU if its firmware version cannot be selected in the hardware catalog of STEP 7 (TIA Portal)?
How do you load the project data if the version of the firmware installed in the S7-1500 CPU cannot be selected in the hardware catalog of your version of STEP 7 (TIA Portal)?
Please note: There will be a "information message" in the module diagnostics, shown beneath "Additional information" ot the online/offline missmatch. This is only an information as in this scenario, the firmware is compatible. regards sancruz |
Feedback appreciated, please rate |
|
Follow us on