9/8/2024 9:28 AM | |
Joined: 11/21/2020 Last visit: 10/11/2024 Posts: 164 Rating: (0) |
Hi, My goal was to connect laptop with 1215C PLC wirelessly using TP-LINK TL-MR3020 wireless router, which is wirelessly conected to my ISP router ZXHN H168N. I managed to connect them, but I had to make additional wireless network using TP-LINK TL-MR3020. The problem was that I had to connect my laptop to TP-LINK TL-MR3020's network in WISP mode instead to ZXHN H168N's wireless network, which left me without the Internet on my laptop. Later I managed to solve the problem by adding D-Link DWA-121 wireless USB adapter to my laptop, but it is overcomplicated. I have noticed that is is irelevant if I use D-Link DWA-121's or laptop's wirelles card in PG/PC interface settings, it works as they are one. All devices, including PLC, are connected to the sam IP v4 network 192.168.1.xxx, with subnet mask 255.255.255.0 Currently I can connect to the PLC using both D-Link DWA-121 and laptop's wireless cards. In project's "online access" list TP-LINK TL-MR3020 is missing, only D-Link DWA-121 and laptop's wireless cards ara available (check an attachment). Is there a way to have both internet and wirelles connection with PLC without using D-Link DWA-121, if yes, which is the simples way to achive it. Thanks
AttachmentWi-Fi PLC.pdf (372 Downloads) |
Last edited by: milos23 at: 09/08/2024 09:33:18 |
|
Follow us on