11/28/2007 3:05 PM | |
Posts: 739 Rating:
|
Dear WAC, when the drive never had switched ON you has to do it! The most important thing is the correct Voltage (If the drive runs continuously you don’t need to do it) find attached a description how to do it.. AttachmentInstallation after a Period of Storage.pdf (837 Downloads) |
11/30/2007 9:11 AM | |
Posts: 739 Rating:
|
Hello William, to reform caps you can use AC-Voltage (mounted on the AC-supply terminals) or DC-Voltage (mounted on DC-Link-Terminals). The needed transformer mustn’t have much “power” (~ 5A max) because the Inverter runs out of load during reforming the caps. The important think here is the use of the correct Voltage; with that voltage the dielectric fluid of the caps will be reformed. If you don’t do that your caps (Inverter) will be destroyed. Link to the FAQ which explains the steps of „reforming caps“http://support.automation.siemens.com/WW/view/en/1960441 |
Follow us on