28.08.2013 11:38 | |
Beiträge: 10 Bewertung:
|
Hello, Matthias. At me the same problem. Look my question in the same section in English. By means of an oscillograph I have understood pins of sockets X141 and X145 on a video card 6FX1154-8BB01. On a socket X141 there are signals R = 6pin, G= 8 pin, B= 10pin, mixed with the synchronisation signals across and verticals. 1,3,7.9 pins – ground. These signals, I think, it is possible to submit on the TV with corresponding inputs or TFT-monitor. But on this socket is still control pin5, from it the signal goes on a microcircuit input on a videocard, likely for control something. On a socket X151 there are 1,3.5.7.9 pins=ground, 2pin = synchronisation signal on a vertical of 60 hertz, 4 pin = a synchronisation signal across 15 kilohertz. 6, 8,10 pins – signals R G B pure, not mixed. I connected this socket to old monitor CGA which supports synchronisation of 15 kilohertz and have received the image. The VGA monitor is not supported, at it frequency of horizontal synchronisation 30 kHz and more. Jumpers = just as on a video card which is described in the Installation Instruction for 820GA3 №338 on page 3-7. I did it on system Sinumerik820GA3. It is possible to look at numbers of the pins of sockets on a small board with numbers, in a monitor compartment, there there is precisely such socket on 16 pins. If you have still any information about this video card, tnenmessage to me. Dateianhang338_810_820_GA3_Installation_Instructions.pdf (145 Downloads) |
Folgen Sie uns auf