(0)| 12/15/2010 10:33 AM | |
|
Joined: 3/4/2009 Last visit: 10/28/2020 Posts: 57 Rating:
|
Hi. I am beginner with step7 basic. I am trying to schedule a daily program from HMI. I want the user to be able to set in HMI the start and stop time for a pump operation. I imagine that i can be done like this: In 4 I/O fields the user sets, for example: Start_1: 08:00 Stop_1: 13:00 Start_2: 18:15 Stop_2: 21:15 if he wants the pump to run every day, from 08:00 to 13:00 and from 18:15 to 21:15. I am not able to configure the I/O fields for the start and stop times. If i get over this, i thing it will be easy to program the plc switching the output, using DTL. Can anybody give an advice? Splitted from Scheduling time clock. |
Last edited by: O_Moderator at: 12/16/2010 11:30 AMnew subject after splitting Last edited by: miltos at: 12/15/2010 10:34 AM |
|
Follow us on