4/7/2018 8:09 AM | |
Posts: 1 Rating: (0) |
i have two cpu s7 1200 .............1st 1214c and 2nd 1212c i want to use one cpu as master and one cpu as slave. is it possible ? if yes then how? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/9/2018 12:17:54 PMNew subject after splitting |
|
4/9/2018 2:46 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051)
|
hi SD0011, for Master-Slave communication you need Profibus-Communication modules. One CPU need the Master-Module CM1243-5 6GK7243-5DX30-0XE0 The other one needs the Slave-module CM1242-5 6GK7242-5DX30-0XE0 the CPUs do also have a Profinet-interface which can be used for the communication between them. therefore one CPU needs to be projected as intellegent IO-device(I-device) for the other. the following application example shows how it works: Configuration and application of PROFINET I-Device function hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
Follow us on