4/27/2023 5:48 PM | |
Joined: 9/2/2022 Last visit: 11/7/2024 Posts: 18 Rating: (0) |
Hello, I have a 2050 Basic FS1 which is not able to boot. After power up, the STAT LED stays solid red. I can't SSH into it as it seems it's not booting. I tried to read any message from the serial terminal so I used an old serial coverter cable that I have. It can be my bad cable, but I see random texts on the screen. Attached a copy of log file. My question is what can be the reason for solid red STAT LED after power up? does any of the words in the log file make sense to you? I'm using the example image V1.1. Thanks in advance ------------------------------------------------------------------------------------------ AttachmentLog.txt (364 Downloads) |
Last edited by: Jen_Moderator at: 04/28/2023 08:24:36New subject after splitting |
|
4/29/2023 3:59 AM | |
Joined: 9/2/2022 Last visit: 11/7/2024 Posts: 18 Rating: (0) |
I was able to get a clear log (attached). it seems the error is : "Card did not respond to voltage select!" AttachmentLog.txt (344 Downloads) |
Follow us on