6/2/2022 7:32 AM | |
Joined: 5/30/2022 Last visit: 6/30/2022 Posts: 2 Rating:
|
Hello, I am an intern electronics engineering (not graduated yet) and got the assignment of fixing the TP1200 comfort(it had been this way before I got it), as I thoroughly researched the way to fixing it such as via Prosave(it wasn't able to find boot HMI device via connecting Ethernet) or USB recovery(which is work only basic panel), My guess is that it might be a problem with electronic hardware or else(with the current small knowledge that I had), so I open the back panel up to check a circuit that is a faulty and I found 3 ceramic capacitors below AMD processor and the other near LTC1628CG are shorted(you can found a picture in the attachment), I not sure it supposed to work this way or not and I don't have access to schematic either even I try to replace those, this is beyond my abilities pls I need help, I try to get any information that can get so I get it fixed and it might help many owners who found this situation. thank you sincerely. Attachmentpicture.pdf (726 Downloads) |
Last edited by: chiawchan at: 06/02/2022 08:21:12 |
|
1/20/2023 1:35 PM | |
Joined: 8/3/2009 Last visit: 8/15/2024 Posts: 13561 Rating:
|
Hello Thanks for sharing but anyway I would send it to repair Center: https://support.industry.siemens.com/cs/ww/en/view/22639376 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on