8/13/2008 11:53 AM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating: (56) |
Hi, This is not possible with the CPU's with integrated ports. For this you need to use the CP's and the special software from Siemens. More information is available here: http://www.industry.siemens.com/IT4Industry/EN/solution_services/simatic_addons/proto_mod.htm?PIdent=1001&SIdent=1018&TIdent=1028&QIdent=1047 |
Best regards, |
|
10/7/2008 10:37 AM | |
Joined: 10/3/2008 Last visit: 12/12/2024 Posts: 966 Rating: (127) |
Hello, the product "S7 OpenMODBUS/TCP PN PLC" is available! The order number is 2XV9450-1MB02. With this product it's possible to communicate via ModbusTCP to third party systems with usage of the integrated PN interface of a PN-CPU. Wüstenräuber AttachmentOpenModbusTCP_eng.pdf (3343 Downloads) |
This contribution was helpful to1 thankful Users |
2/16/2009 1:13 PM | |
Posts: 94 Rating: (15) |
Hi , It is possible to connect the modbus TCP connection with integrated port. I have attached here the link for open modbus TCP Wizard. Check with that. http://support.automation.siemens.com/WW/view/en/31535566 Titas |
Follow us on