5/9/2011 11:19 AM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating: (86) |
Hi well i had the similar problem when i connected a 4 wire to 1KF 02 card, It used to read 16#8000 only when increase the mA above say 10mA it used to vary a little. Then later i found that the wiring for the 1KF01 and 1KF02 are little diffrent. the "M" negative of the 24 V is to be looped at all the points in the card and given to electronic earth. and the signal cable has to be earthed properly at the field side. After i did that my problem got solved. Have fun.. |
Jazz |
|
This contribution was helpful to1 thankful Users |
Follow us on