5/1/2018 3:44 AM | |
Joined: 4/28/2015 Last visit: 5/9/2024 Posts: 15 Rating:
|
Hi, I do not have enough English, but I have a question for you. I use 416-5H CPUs. I completed the commissioning in Kuwait a year ago. But there's a problem, a year later ... I am using RAM memory. So I checked the battery, but it was normal. I tried to download the program again, but I could not download it. I had factory reset. After that I succeeded in downloading the program. However, after that, the CPU stopped because of the following error. If you put the program into the simulator and start up, it will work normally. Add. "Event 4303 " is the event where the field operator manipulated the stop key. It's in a state similar to when the problem occurred. Below is the diagnosis at the time of the first occurrence of the problem. --------------------------------------------- PLC LED Status : Master CPU - EXTF, STOP, REDF, MSTR, RACK0 Backup CPU - EXTF, STOP, REDF, RACK1 Event 1 of 120: Event ID 16# 43F1 Switchover of master CPU and standby CPU Previous operating mode: STOP (internal) Requested operating mode: STOP (internal) Event occurred in the standby CPU in rack 1 Incoming event 12:17:25.221 PM 04/24/2018 (Coding: 16# 43F1 F144 0000 0000 0000 0000) Event 2 of 120: Event ID 16# 49A4 STOP: inconsistency in the configuration data occurred when checking Parameters for internal consistency No consistency entries assignable Error type: Time stamps of the loaded parameter fields do not match Previous operating mode: STOP (internal) Requested operating mode: STOP (internal) Event occurred in the master CPU in rack 0 External error, Incoming event 12:17:22.491 PM 04/24/2018 (Coding: 16# 49A4 F844 C17B 0004 0000 0131) Event 3 of 120: Event ID 16# 530D New startup information in STOP mode Startup prevented by: Loading user program or internal inconsistency detected (SDBs less than 200 incomplete, superfluous, or incorrect) - Cold restart or warm restart necessary Startup information: - Time for time stamp at the last backed up power on - Single processor operation Current/last startup type: - No startup type/following memory reset Permissibility of certain startup types: - Manual warm restart permitted Last valid operation or setting of automatic startup type at power on: - No startup type/following memory reset Operating mode: STOP (internal) Event occurred in the master CPU in rack 0 Incoming event 12:17:22.491 PM 04/24/2018 (Coding: 16# 530D F804 C777 0140 0800 0700) Event 4 of 120: Event ID 16# 4303 STOP caused by stop switch being activated Previous operating mode: STOP (internal) Requested operating mode: STOP (internal) Event occurred in the master CPU in rack 0 Incoming event 12:17:20.960 PM 04/24/2018 (Coding: 16# 4303 F844 0000 0000 0000 0000) ------------------------------------------------- Below is the diagnosis after re-downloading. I attach the cfg file extracted from the editor, and diagnosis data. ----------------------------------------------------- PLC LED Status : Master CPU - EXTF, STOP, REDF, MSTR, RACK0 Backup CPU - EXTF, STOP, REDF, RACK1 Diagnostic buffer of module CPU 416-5 H PN/DP " Order No./ Description Component Version 6ES7 416-5HS06-0AB0 Hardware 1 - - - Firmware V 6.0.1 Boot Loader Firmware expansion V 6.0.0 Rack: --- Slot: --- Serial number: SVPCD678864 Event 1 of 15: Event ID 16# 49A4 STOP: inconsistency in the configuration data occurred when checking Parameters for internal consistency No consistency entries assignable Error type: Time stamps of the loaded parameter fields do not match Previous operating mode: STOP (internal) Requested operating mode: STOP (internal) Event occurred in the master CPU in rack 0 External error, Incoming event 01:44:12.532 AM 01/01/1994 (Coding: 16# 49A4 F844 C17B 0004 0000 0131) Event 2 of 15: Event ID 16# 530D New startup information in STOP mode Startup prevented by: Loading user program or internal inconsistency detected (SDBs less than 200 incomplete, superfluous, or incorrect) - Cold restart or warm restart necessary Startup information: - Time for time stamp at the last non backed up power on - Single processor operation Current/last startup type: - No startup type/following memory reset Permissibility of certain startup types: - Manual warm restart permitted Last valid operation or setting of automatic startup type at power on: - No startup type/following memory reset Operating mode: STOP (internal) Event occurred in the master CPU in rack 0 Incoming event 01:44:12.532 AM 01/01/1994 (Coding: 16# 530D F804 C777 0140 0000 0700) Event 3 of 15: Event ID 16# 4303 STOP caused by stop switch being activated Previous operating mode: STOP (internal) Requested operating mode: STOP (internal) Event occurred in the master CPU in rack 0 Incoming event 01:44:12.262 AM 01/01/1994 (Coding: 16# 4303 F844 0000 0000 0000 0000) Event 4 of 15: Event ID 16# 49A4 STOP: inconsistency in the configuration data occurred when checking Parameters for internal consistency No consistency entries assignable Error type: Time stamps of the loaded parameter fields do not match Previous operating mode: STOP (internal) Requested operating mode: STOP (internal) Event occurred in the master CPU in rack 0 External error, Incoming event 01:42:51.466 AM 01/01/1994 (Coding: 16# 49A4 F844 C17B 0004 0000 0131) Event 5 of 15: Event ID 16# 530D New startup information in STOP mode Startup prevented by: Loading user program or internal inconsistency detected (SDBs less than 200 incomplete, superfluous, or incorrect) - Cold restart or warm restart necessary Startup information: - Time for time stamp at the last non backed up power on - Single processor operation Current/last startup type: - No startup type/following memory reset Permissibility of certain startup types: - Manual warm restart permitted Last valid operation or setting of automatic startup type at power on: - No startup type/following memory reset Operating mode: STOP (internal) Event occurred in the standby CPU in rack 0 Incoming event 01:42:51.466 AM 01/01/1994 (Coding: 16# 530D F004 C777 0140 0000 0700) Event 6 of 15: Event ID 16# 43F1 Switchover of master CPU and standby CPU Previous operating mode: STOP (internal) Requested operating mode: STOP (internal) Event occurred in the standby CPU in rack 0 Incoming event 01:42:51.464 AM 01/01/1994 (Coding: 16# 43F1 F044 0000 0000 0000 0000) Event 7 of 15: Event ID 16# 530D New startup information in STOP mode Startup prevented by: Loading user program or internal inconsistency detected (SDBs less than 200 incomplete, superfluous, or incorrect) - STOP request exists - Keyswitch set to STOP - Cold restart or warm restart necessary Startup information: - Time for time stamp at the last non backed up power on - Single processor operation Current/last startup type: - No startup type/following memory reset Permissibility of certain startup types: - Manual warm restart permitted Last valid operation or setting of automatic startup type at power on: - No startup type/following memory reset Operating mode: STOP (internal) Event occurred in the standby CPU in rack 0 Incoming event 01:42:51.464 AM 01/01/1994 (Coding: 16# 530D F004 C777 0161 0000 0700) Event 8 of 15: Event ID 16# 4303 STOP caused by stop switch being activated Previous operating mode: STOP (internal) Requested operating mode: STOP (internal) Event occurred in the standby CPU in rack 0 Incoming event 01:42:50.983 AM 01/01/1994 (Coding: 16# 4303 F044 0000 0000 0000 0000) Event 9 of 15: Event ID 16# 43F1 Switchover of master CPU and standby CPU Previous operating mode: STOP (internal) Requested operating mode: STOP (internal) Event occurred in the standby CPU in rack 1 Incoming event 12:01:14.093 AM 01/01/1994 (Coding: 16# 43F1 F144 0000 0000 0000 0000) Event 10 of 15: Event ID 16# 49A4 STOP: inconsistency in the configuration data occurred when checking Parameters for internal consistency No consistency entries assignable Error type: Time stamps of the loaded parameter fields do not match Previous operating mode: STOP (internal) Requested operating mode: STOP (internal) Event occurred in the master CPU in rack 0 External error, Incoming event 12:01:10.307 AM 01/01/1994 (Coding: 16# 49A4 F844 C17B 0004 0000 0131) Event 11 of 15: Event ID 16# 530D New startup information in STOP mode Startup prevented by: Loading user program or internal inconsistency detected (SDBs less than 200 incomplete, superfluous, or incorrect) - Cold restart or warm restart necessary Startup information: - Time for time stamp at the last non backed up power on - Single processor operation Current/last startup type: - No startup type/following memory reset Permissibility of certain startup types: - Manual warm restart permitted - Automatic warm restart permitted Last valid operation or setting of automatic startup type at power on: - Automatic warm restart after non backed up power on (with system memory reset) Operating mode: STOP (internal) Event occurred in the master CPU in rack 0 Incoming event 12:01:10.307 AM 01/01/1994 (Coding: 16# 530D F804 C777 0140 0000 7720) Event 12 of 15: Event ID 16# 530D New startup information in STOP mode Startup prevented by: - Cold restart or warm restart necessary Startup information: - Time for time stamp at the last non backed up power on - Single processor operation Current/last startup type: - No startup type/following memory reset Permissibility of certain startup types: - Manual warm restart permitted - Automatic warm restart permitted Last valid operation or setting of automatic startup type at power on: - Automatic warm restart after non backed up power on (with system memory reset) Operating mode: STOP (internal) Event occurred in the master CPU in rack 0 Incoming event 12:01:10.303 AM 01/01/1994 (Coding: 16# 530D F804 C777 0040 0000 7720) Event 13 of 15: Event ID 16# 43F1 Switchover of master CPU and standby CPU Previous operating mode: STOP (own initialization) Requested operating mode: STOP (own initialization) Event occurred in the master CPU in rack 0 Incoming event 12:01:06.058 AM 01/01/1994 (Coding: 16# 43F1 F833 0000 0000 0000 0000) Event 14 of 15: Event ID 16# 430E Memory reset executed Initialization information: Memory reset due to inconsistent data Previous operating mode: STOP (memory reset) Requested operating mode: STOP (own initialization) Event occurred in the standby CPU in rack 0 Incoming event 12:01:00.925 AM 01/01/1994 (Coding: 16# 430E F023 CE00 0000 0000 0008) Event 15 of 15: Event ID 16# 4309 Memory reset started automatically (power on not backed up ) Initialization information: Memory reset due to inconsistent data No relevance for user (Z1): 0001 Previous operating mode: No voltage Requested operating mode: STOP (memory reset) Event occurred in the standby CPU in rack 0 Incoming event 12:01:00.913 AM 01/01/1994 (Coding: 16# 4309 F0F2 CE50 0001 0000 0008) AttachmentHardware and Diagnose.zip (172 Downloads) |
Last edited by: AutoGen_788039 at: 5/1/2018 3:47:32 AMLast edited by: AutoGen_788039 at: 5/1/2018 5:38:10 AM |
|
5/1/2018 10:06 PM | |
Joined: 1/28/2009 Last visit: 8/5/2024 Posts: 6844 Rating:
|
Dear user, Please check if your CPU needs a long time to perform the start up.Use a Stop-watch to measure this time.The key problem is Event ID :49A4,you will find more details in attached file. Best regards, hdhosseini Attachment49A4.txt (765 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on