8/4/2022 3:17 PM | |
Joined: 1/21/2013 Last visit: 8/4/2024 Posts: 3044 Rating: (479) |
Hi steemm, the ET 200SP F-DI 8x24VDC HF (6ES7136-6BA01-0CA0) is the successor to the ET 200SP F-DI 8x24VDC HF (6ES7136-6BA00-0CA0). As you can find in the release note, this is done with full replacement part compatibility. This means, you can use the module and still configure the old one. The only restriction is, that you are not able to use the new features in this case. To configure the new module, you would need at least TIA Portal V17. Kind regards |
This contribution was helpful to3 thankful Users |
Follow us on