6/4/2010 1:22 PM | |
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
You need Drive Monitor cable for that You can find Pin Configuration in Manual RS 232 will not work Regards, Devesh AttachmentDriveMonitorCable.pdf (407 Downloads) |
Last edited by: Vithani at: 6/4/2010 1:23 PMI attached PIN configuration I dont Like people driving Fast, thats the reason I overtake them ;) |
|
6/4/2010 1:25 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, Means you have DriveMonitor Version V5.4 SP2 for SIMOVERT MASTERDRIVES, MICROMASTER and SIMOREG. Start Drive Monitor. Go to Tools - Online settings. There select - Bus Type - USS, Interface RS232 COM1 (or actual COM port) baud rate 9600 (you could try also 19200). Close settings. Then go to File - Setup an USS online connection. Mark Open the first fond drive immediately online and push start. If everything is OK (should be) the program will automatically will recognize the type of drive and will open it. best regards, Hristo Mihalev |
6/4/2010 1:26 PM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hi, Thanks for your reply. With regards, DEEP. |
Follow us on