1/22/2022 10:02 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello, 6sl3210-5fb10-8ua0 is Sinamics V90, 0.75 KW 200 V drive. Compatible motors with these drives are SIMOTICS S-1FL6 motors only. Which motor you want to connect? Please check its compatibility with V90 drive, refer SINAMICS V90 Pulse train, USS/Modbus, SIMOTICS S-1FL6 Operating Instructions manual for more details. P. S. - X8 is 50 pin socket for control/status interface & not for brake connection. Motor holding brakes are connected to X7 connector. |
Last edited by: PISCEAN 2010 at: 01/22/2022 10:18:56P. S. added |
|
1/22/2022 11:04 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Connect to X7 connector. Refer attached sheet. |
1/22/2022 11:09 AM | |
Joined: 10/24/2016 Last visit: 6/14/2024 Posts: 57 Rating:
|
I have the driver pictured attached. no x7 connector |
1/22/2022 11:42 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Motor which you specified does not have brake. Please check. 1FL6042-2AF21-1AA1 (EAN: 4042948670910 / UPC: 804766254864) SERVOMOTOR 1FL6;3AC 230V SIMOTICS S-1FL6 Operating voltage 230 V 3AC Pn=0.75 kW; Nn=3000 rpm M0=2.39 Nm; MN=2.39 Nm Shaft height 40 mm Incremental encoder TTL 2500 incr./rev. with feather key Tolerance N without holding brake Degree of protection IP65 with sealing ring compatible with the converters SINAMICS V90
|
Follow us on