Industry Online Support
Technical Forum
6/23/2010 7:18 PM | |
Posts: 3 Rating: (0) |
Hi So i have partially solve my problem, the solution i have come up whit are : 1. The first one was to move the pusher beside the sensor, so i had to use only a timer ( a easy solution :D ) 2. For the next one, i kept the distance 'x' between the sensor and the pusher, and the speed of the conveyor line constant ( v = ct ), I use counter's, comparators, and timer's, below is an example of the program, i use step 7 because it's easy to use especially the simulator. 3. The 3 one is the hardest for me, because i want to kept count of the line speed, so i have anther input that keep count of the conveyor. To be honest i am stuck, because i don't know what to use, i solve the problem whit multiple cube's that pas the sensor , but don't know how to implement the counter that keeps track of the speed If anyone has same ideas, i will gladly listen :) Attachmentprogram S7 pusher, distanta constanta.pdf (406 Downloads) |
Follow us on