12/1/2017 9:24 AM | |
Posts: 80 Rating: (2) |
Hi, I am trying to build my own image with the meta-iot2000-bsp layer following the instructions of the Readme. A customer is also trying to build his own image and it is not succeeding. Please, I need to help him, I need a clear way of how to build the image. The build failed and in the log says that acpi-upgrades-iot2000.cpio is invalid. What can be the problem? The steps I have followed are: $ sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib build-essential chrpath socat libsdl1.2-dev xterm $ pip3 install kas $ kas build meta-iot2000-bsp/kas.yml AttachmentImage creation error.zip (165 Downloads) |
Last edited by: Laura_Martin at: 12/1/2017 9:26:16 AM |
|
12/1/2017 1:01 PM | |
Posts: 80 Rating: (2) |
I have retried the build with the previous results but nothing changes. I have attached the log.do_bootimg.13806 file to the .zip.
AttachmentImage creation error.zip (145 Downloads) |
12/1/2017 3:05 PM | |
Joined: 4/28/2015 Last visit: 4/21/2024 Posts: 578 Rating: (43) |
Ok, this could have actually been a dependency issue. I've pushed a fix to https://github.com/siemens/meta-iot2000/tree/jan/bootimg-dep-fix Looking forward to hear if that helps. Thanks for reporting! |
Last edited by: jan-k at: 12/1/2017 3:06:23 PM |
|
12/5/2017 12:42 PM | |
Posts: 80 Rating: (2) |
I have a problem when trying to build the image with this new meta-iot2000. I think it is a problem with paths, somewhere, it add one more layer to the path. Attached there ir the conf file of the layers and the error.
AttachmentError.zip (190 Downloads) |
12/7/2017 6:42 PM | |
Joined: 4/28/2015 Last visit: 4/21/2024 Posts: 578 Rating: (43) |
Meanwhile, I've succeeded with reproducing the issue and issued https://github.com/siemens/meta-iot2000/pull/65. When you test, please use that version to avoid being bit by yet another build failure after the first one was fixed. |
Follow us on