5/16/2014 11:45 AM | |
Joined: 7/2/2008 Last visit: 7/2/2024 Posts: 928 Rating: (306) |
Hellokhaksar,
How do you try to connect to both CPUs? Do you have Ethernet connection? Do you have MPI connection?In this case do you have MPI cable connecting both CPUs together?Do you have different MPI addresses in both CPUs? What kind of memory cards do you have FLASH or RAM?
As far as I remember this is a normal behavior. When both CPUs are running without FO connection, both are becoming MASTER. You can't connect the FO all of a sudden. You should STOP one of them. connect the FO and then run the one in STOP. for a 414-4H, do not open any variable table during this procedure. The most important thing will be your diagnostic buffer. So, if you are still having problems, please upload your diagnostic buffer. Best regards, H-H
|
This contribution was helpful to1 thankful Users |
Follow us on