Industry Online Support
Technical Forum
10/6/2010 9:31 PM | |
Posts: 33 Rating: (0) |
Hi Guys I have two problems and possibiltities. Firstly and most annoyingly, my Display has a continous popup where there are alarms and after sorting all of them out, the box stays there, show the value of 0 because there are no alarms and doesnt go away. how can i get it to disappear when there are no alarms or even move the location of it so it pops up somewhere else. [schnippschnapp] second question is splitted to i set bit m5.5 in plc for a low level alarm and i get a high level alarm which is on another bit. Help?!? |
Last edited by: O_Moderator at: 10/11/2010 9:43 AMLast edited by: Andy Moods at: 10/6/2010 9:34 PM |
|
10/31/2010 9:20 AM | |
Posts: 33 Rating: (0) |
Hi The box has a vaue of 0 and there are no alarms present but the box is still displayed. |
11/1/2010 2:51 PM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147) |
Hello, Are all alarms Acknowledged? Best regards, Wizard |
Follow us on