1/18/2011 8:26 AM | |
Posts: 15 Rating: (1) |
Nobody? Realy? |
2/3/2011 2:31 AM | |
Joined: 10/7/2005 Last visit: 10/14/2024 Posts: 3024 Rating: (1054)
|
Hello Borut23 perhaps a bit late, but it may still help you now and/or in similar applications in the future: The lastest S7 PN CPU's (finally) support so called "I-device" functionality. What this means is that they can act as a Profinet I/O Controller as well as an intelligent Profinet I/O device at the same time. You could then have one CPU as an I-device of the "main" CPU and exchangevalues between them via Profinet I/O's. This will be much faster than any Send/Receive or S7 communciation based linkthat you can configure/program betweenthem and you can find out more about it at the link below: Which CPU can you operate as a PROFINET I device? I hope this helps |
Cheers |
|
This contribution was helpful to1 thankful Users |
Follow us on