3/22/2018 8:34 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hi royalmaster, the FAQ "How do you create your own block icons with SIMATIC PCS 7?" describe how do you create your own block icons on a motor block. With regards |
4/2/2018 5:25 AM | |
Joined: 9/9/2015 Last visit: 10/28/2024 Posts: 728 Rating: (280) |
To do so, you can pull a static text from the tool in graphic designer, right click at the "text" in properties, add a dynamic dialog. For this, you can set boolean (if you have only Running and stopped), or set analog (if you have more than one status). If you wanna change the color, go to the color, background color, and add a dynamic dialog there. If you wanna hav the rectangle box, set the static text border to have line weight of 1 . Hope it helps. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on