Industry Online Support
Technical Forum
11/11/2013 4:42 PM | |
Joined: 5/18/2006 Last visit: 10/21/2020 Posts: 170 Rating: (64) |
With PCS 7 V8.0 SP1 there is no need to modify or write your own script inorder to open the APL Faceplate Trend window in the archive/history mode. See attached (extracted from the PCS 7 V8.0 SP 1 Manual Collestion). All that is required is to place a SemiColon follwed by a 1 in the block icon property 'TrendPictureName' (e.g. @pg_apl_TrendPID_Statistic.pdl;1). cabreytj AttachmentD:\Users\cabrtj\PCS_7_V8.0_SP_1_Manual_Collection_-_Trend_view[1].pdf (165 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on